Press Arrow button (1) repeatedly until the setting mode LED (3) has a steady green light. The actual time indicator (6) has a flashing yellow light.

Press the Change button (8) repeatedly until the time LED reaches the current time (4:30 PM in this example). Note: The LED moves more quickly if the setting button (8) is held down.

Press OK (9) to confirm. The time LED (6) now has a steady yellow light. The actual time has been set. The operating time LED (7) 0:00 – 0:30 AM has a flashing green light and already selected operating times are indicated.

Press Arrow button (1) to exit setting mode. Timer mode LED (4) lights up. The actual time and already selected operating times are indicated.