LED (2) steady green light. Pump operates in AUTOADAPT mode.

LED (2) flashes green light. Pump is stopped and waiting in AUTOADAPT mode for condition to resume operation (e.g. water to cool down, time of the day when is predicted for water to be used or tapping detection if it is in vacation mode)

LED (2) AUTODAPT has steady green or flashing light, depending on conditions. LED (5) Warning has steady yellow light. External sensor is broken. Pump operates in temperature mode based on only internal sensor. Vacation mode is not possible.